15.10.8 Displaying Pins in a VREF Range
You can see which pins in an I/O bank are serviced by a VREF pin. Use the right-click menu's Highlight VREF Range command while in PinEditor or ChipPlanner to see these pins.
To display pins in a VREF range:
- Right-click a VREF pin in either PinEditor or ChipPlanner.
- From the right-click menu, choose Highlight VREF Range.
When using PinEditor, all pins serviced by the selected VREF pin appear highlighted.
When using ChipPlanner, all I/O modules serviced by the selected VREF pin appear highlighted.
To highlight all pins in a VREF range:
- Right-click an I/O bank in either PinEditor or ChipPlanner.
- From the right-click menu, choose Highlight All Pins in a VREF Range.
The HighlightAll Pins in a VREF Range command appears in the right-click menu for all I/O banks that include a VREF pin.
All of the pins in the I/O bank that are serviced by a VREF appear highlighted. If the I/O bank does not contain a VREF pin, nothing is highlighted when you select this command.
To unhighlight all pins in a VREF range:
- Select the highlighted range.
- From the Edit menu, choose Unhighlight All.