5.33.7 Lists and arrays
A list is a way to group data and handle the group as a single entity. To define a list, use curly braces { } and double quotes “ “. For example, the following set command {1 2 3 }, when followed by the list command, creates a list stored in the variable "a." This list will contain the items "1," "2," and "3."
set a { 1 2 3 }
Here's another example:
set e 2
set f 3
set a [ list b c d [ expr $e + $f ] ] puts $a
displays (or outputs):
b c d 5
Tcl supports many other list-related commands such as lindex, linsert, llength, lrange, and lappend. For more information, refer to one of the books or web sites available on this subject.