5.7.4 Startup Tab

Several programs, including the Libero IDE Project Manager, create files with the PRJ extension. If you want the Project Manager to start whenever you double-click a PRJ file, you need to set up Project Manager as the default editor for PRJ files.

You must have rights to modify the HKEY_CLASSES_ROOT of the registry of the machine to set Libero IDE Project Manager file association. If you do not have rights to modify the registry, Libero IDE ignores your settings.

To make the Project Manager the default editor for PRJ files:

  1. From the Project menu, choose Preferences.
  2. Click the Startup tab.
  3. Select the check box to associate Libero IDE Project Manager with PRJ files.

To open the most recently used project at startup:

  1. From the Project menu, choose Preferences.
  2. Click the Startup tab.
  3. Select the check box to open the most recently used project at startup.