13.21.5 Removing Bus Interfaces from Instances
Only bus interfaces that you explicitly added to an instance can be removed or deleted. Bus interfaces that were instantiated as part of core generation cannot be deleted.
To delete user added bus interfaces, on the Canvas , select the bus interface pin object, right-click, and choose Delete Bus Interface; or, in the Grid, select the Port Name field, right-click, and choose Delete Bus Interface.