20.4.2.1 Arguments
-type power_peak_analyzer
Specifies the type of report to generate is a cycle accurate power report.
-vcd_file {path}
Specifies the path to the *.vcd file that you want to import.
-style {value}
Specifies the format in which the report will be exported. The following table shows the acceptable values for this argument:
Value |
Description |
|---|---|
Text |
The report will be exported as Text file |
CSV |
The report will be exported as CSV file |
-partial_parse {value}
Specifies whether to partially parse the *.vcd file. The following table shows the acceptable values for this argument:
Value | Description |
|---|---|
true | Partially parses the *.vcd file |
false | Does not partially parse the *.vcd file |
-start_time {value}
This option is available only if -partially_parse is set to true. Specifies the start time (in ns) to partially parse the *.vcd file.
-end_time {value}
This option is available only if -partially_parse is set to true. Specifies the end time (in ns) to partially parse the *.vcd file.
-auto_detect_top_level_name {value}
Specifies whether to automatically detect the top-level name. The following table shows the acceptable values for this argument:
Value | Description |
|---|---|
true | Automatically detects the top-level name |
false | Does not automatically detect the top-level name |
-top_level_name {name}
Specifies the top-level name.
-glitch_filtering {value}
Specifies whether to use glitch filtering. The following table shows the acceptable values for this argument:
Value | Description |
|---|---|
true | Glitch filtering is on |
auto | Enables automatic glitch filtering. This option will ignore any value specified in -glitch_threshold |
false | Glitch filtering is off |
-glitch_threshold {value}
This option is only available when -glitch_filtering is set to true. Specifies the glitch filtering value (in ps).
-power_summary {value}
Specifies whether to include the power summary, which shows the static and dynamic values in the report. The following table shows the acceptable values for this argument:
Value | Description |
|---|---|
true | Includes the power summary in the report |
false | Does not include the power summary in the report |
-auto_detect_sampling_period {value}
Specifies whether to automatically detect the sampling period. The following table shows the acceptable values for this argument:
Value | Description |
|---|---|
true | Automatically detects the sampling period |
Value | Description |
|---|---|
false | Does not automatically detect the sampling period |
-sampling_clock {}
Specifies the sampling clock.
-sampling_rate_per_period {value}
Specifies whether to set the sampling rate per period. The following table shows the acceptable values for this argument:
Value | Description |
|---|---|
true | Specifies the sampling rate per period |
false | Specifies the sampling rate per half period |
-sampling_offset {value}
Specifies the offset used to calculate the sampling offset (in ps).
-sampling_period {value}
Specifies the offset used to calculate the sampling period (in ps).
-use_only_local_extrema {value}
Specifies whether to limit the history size by keeping only local extrema. The following table shows the acceptable values for this argument:
Value | Description |
|---|---|
true | Limits the history size by keeping only local extrema |
false | Does not limit the history size by keeping only local extrema |
-use_power_threshold {value}
Specifies whether to limit the history size by setting a power threshold. The following table shows the acceptable values for this argument:
Value | Description |
|---|---|
true | Limits the history size by setting a power threshold |
false | Does not limit the history size by setting a power threshold |
-power_threshold {value}
Sets the power threshold value.
-opmode {value}
Use this option to specify the mode from which the operating conditions are extracted to generate the report.
{filename}
Specifies the name of the report.