13.6.7.3.1 Warn me before:

  • Simulation of the wrapper of an IP core - Simulation of the top-level wrapper is incomplete relative to simulation of the core itself. Click the checkbox to enable a warning when you simulate a wrapper. Actel recommends that you run simulation on the core, and run synthesis on the wrapper (see warning below).
  • Synthesis of an IP core - Synthesis of the core is incomplete relative to synthesis of the wrapper. Click the checkbox to enable/disable a warning if you synthesize an IP core instead of the wrapper. Actel recommends that you run synthesis on the wrapper, and run simulation on the core (see warning above).
  • Launching a tool on a component with errors - De-select this option to prevent warnings when you launch a tool on a component that has errors in it. This may be useful if you wish to leave some elements of the component incomplete and finish them at a later time. If you de-select this option, you will not have to see a warning every time you open the component.
  • Launching a tool on an out of date component - De-select this option if you do not wish to see warning messages related to out of date components. A component is out of date if a newer version is available.