9.9.1 Selecting an Action

The actions you have available are based upon what type of STAPL file you have loaded into the software.

To configure a programmer:

  1. From the Configure menu, choose Select Action and Procedures. The Select Action and Procedures dialog box appears.
    Figure 9-116. Select Action of Procedures Dialog Box
    ???
  2. Click the checkboxes of the available procedures or click the Restore Default Procedures button in the Select Action and Procedures dialog box.
  3. Click OK.

Click the Restore Default Procedures to return to default settings.