13.8.5 Designer Blocks and Synthesis
You must run the synthesis tool in No I/O mode when you create your component. The Designer Block is not a full design; Libero IDE sets this option for Synplify if you Enable Designer Block creation.
When you Publish a Designer Block, the Project Manager creates a timing shell that enables the
synthesis tool to better synthesize the <top> project. The timing shell is named
<blockname>_syn.v(.vhd) if you are using Synplify or
<blockname>_pre.v(.vhd) if you are using Precision.
When you are working in your <top> project, the synthesis tool does not know how many globals you have in your Designer Block, or if there will be clock sharing. The synthesis tool promotes as many globals as it can (example, four globals for Axcelerator devices) and if you have globals in the Designer Block you will exceed the total number of globals allowed in your device.
In this case, you must limit the number of globals added by the synthesis tool so that the total number (Designer Block plus <top> project) does not exceed the number available on your device.
To add an internal global, you can use either the Synplify constraints editor (SCOPE) or an SDC file. For example, to add a CLKINT after a CLK port, the command is:
define_attribute {n:CLK} syn_insert_buffer {CLKINT}