7.4.3 Adding Pins to the Design
Add pins to the top-level schematic of the design by using the I/O buffer cores with a dangling net attached to the pad, as shown in the following figure. The label on the dangling net becomes the I/O pin name.
Add pins to the top-level schematic of the design by using the I/O buffer cores with a dangling net attached to the pad, as shown in the following figure. The label on the dangling net becomes the I/O pin name.
Rev: A