3.4.3.5 ID Check
ID Check Overview
The ID check module can compare predefined IDs with the first bytes of the received data payload. If a match occurs, this is indicated in a single register bit. The ID can have a length of 1, 2, 3 or 4 bytes and an offset from the beginning of the data payload of 0, 1, 2 or 3 bytes. The block is controlled by an internal finite state machine.
To initiate an ID check, the required ID must first be written to the ID byte registers IDB0, IDB1, IDB2 and IDB3. An ID can therefore have a length of 1, 2, 3 or 4 bytes which must be configured in the IDC.IDL register. If the ID is not located at the very beginning of the data payload, a byte-wise offset of up to 3 bytes can be configured in IDC.IDBO.
Before the ID check is started, the user must ensure that at least the IDC.IDBO + IDC.IDL payload bytes have been received, because otherwise the ID check will fail.
The user can enable an ID buffer full interrupt by setting IDC.IDFIM to ‘1’.
This triggers an interrupt to the AVR after 7 bytes are received, which is the worst case
scenario (ID length of 4 bytes and 3 bytes offset). The interrupt can be used by the software
to start an ID check with any configuration regardless of the length and offset values of the
actual ID. Instead of using the interrupt, the IDS.IDFULL flag can be polled.
After the configuration is complete, the ID check can be started by setting IDC.IDCE to
‘1’. It is permitted to write IDCE together with IDBO and IDL in one write
access to the IDC register. The result is available within one clock cycle and written to
IDS.IDOK. A ‘1’ marks a successful ID check. The bit is only cleared by a
module reset or by writing a ‘1’ to it, but not by a successive negative ID
check. This functionality allows an arbitrary number of IDs to be processed in a row, and
checking afterward if at least one match occurred.
The ID check is reset when activated in the corresponding PRR2.PRIDS power reduction register
(see Sleep Modes and Active Power Reduction) or by writing a
‘1’ to the IDC.IDCLR bit.
If not stated otherwise, a detailed description of the required register bits is found in ID Check Register Description.