1.1.3.4.19 DRV_RF215_READY_STATUS_CALLBACK Typedef
C
typedef void ( *DRV_RF215_READY_STATUS_CALLBACK ) (uintptr_t context, SYS_STATUS status);
Summary
Pointer to a RF215 driver ready status callback function.
Description
This data type defines the required function signature for the RF215 driver ready status event handling callback function. A client uses DRV_RF215_ReadyStatusCallbackRegister to register a pointer to a function which must match the signature (parameter and return value types) specified by this data type.
Parameters
| Param | Description |
|---|---|
| context | Value identifying the context of the client that registered the callback function. |
| status | SYS_STATUS_READY or SYS_STATUS_ERROR, depending on initialization result. |
Returns
None.
Example
static void APP_ReadyNotCb(uintptr_t ctxt, SYS_STATUS status) { DRV_HANDLE drvRf215Handle; // The context handle was set to an application specific object // It is now retrievable easily in the event handler MY_APP_OBJ myAppObj = (MY_APP_OBJ *) ctxt; if (status == SYS_STATUS_READY) { // Driver ready to be opened. drvRf215Handle = DRV_RF215_Open(DRV_RF215_INDEX_0, RF215_TRX_ID_RF09); } } MY_APP_OBJ myAppObj; // Application specific data object DRV_RF215_ReadyStatusCallbackRegister(APP_ReadyNotCb, (uintptr_t) myAppObj);
Remarks
The context parameter contains a handle to the client context, provided at the time the callback function was registered using DRV_RF215_ReadyStatusCallbackRegister. This context value is passed back to the client as parameter. It can be any value necessary to identify the client context or instance (such as a pointer to the client's data) of the client that registered the callback.