1.1.3.4.38 DRV_RF215_PHY_TYPE_CFG_OBJ Union
C
typedef union
{
DRV_RF215_FSK_CFG_OBJ fsk;
DRV_RF215_OFDM_CFG_OBJ ofdm;
} DRV_RF215_PHY_TYPE_CFG_OBJ;Summary
Defines the data required to configure the RF215 FSK/OFDM PHY.
Description
This data type defines the data required to configure the parameters associated to the corresponding RF215 PHY (FSK or OFDM).
This is a static PHY configuration, meaning that a RF215 device will only receive messages if the configuration is the same as in the transmitter.
Field description:
- fsk: FSK PHY configuration (see DRV_RF215_FSK_CFG_OBJ)
- ofdm: OFDM PHY configuration (see DRV_RF215_OFDM_CFG_OBJ)
Remarks
None.