1.1.3.4.5 DRV_RF215_Open Function
C
DRV_HANDLE DRV_RF215_Open (
const SYS_MODULE_INDEX index,
const DRV_RF215_TRX_ID trxID
);Summary
Opens the specified RF215 driver instance and returns a handle to it.
Description
This routine opens the specified RF215 driver instance and provides a handle that must be provided to all other client-level operations to identify the caller and the instance of the driver. The trxID parameter defines the RF215 transceiver (Sub-GHz or 2.4GHz) used by the client.
Precondition
Function DRV_RF215_Initialize must have been called and function DRV_RF215_Status should have returned SYS_STATUS_READY before calling this function.
Parameters
| Param | Description |
|---|---|
| index | Identifier for the object instance to be opened. Only one instance (index 0) supported. |
| trxID | Identifier of the RF215 transceiver (Sub-GHz or 2.4GHz) used by the client. |
Returns
If successful, the routine returns a valid open-instance handle (a number identifying both the caller and the module instance).
If an error occurs, the return value is DRV_HANDLE_INVALID. Error can occur
- if the number of clients allocated via MCC is insufficient.
- if the specified instance index is not supported.
- if the specified RF215 transceiver is not supported or disabled via MCC.
- if the driver instance being opened is not ready to be opened (not initialized, initialization in progress or in error state because of wrong peripheral/hardware configuration).
Example
SYS_MODULE_OBJ sysObjDrvRf215; // Returned from DRV_RF215_Initialize
SYS_STATUS drvRf215Status;
DRV_HANDLE drvRf215Handle;
drvRf215Status = DRV_RF215_Status(sysObjDrvRf215);
if (drvRf215Status == SYS_STATUS_READY)
{
// This means now the driver can be opened using DRV_RF215_Open routine
drvRf215Handle = DRV_RF215_Open(DRV_RF215_INDEX_0, RF215_TRX_ID_RF09);
if (drvRf215Handle != DRV_HANDLE_INVALID)
{
// Driver opened successfully
}
}Remarks
The handle returned is valid until the DRV_RF215_Close routine is called.