2.1.4.1 DRV_MCMETROLOGY_Initialize Function
C
Returns
SYS_MODULE_OBJ DRV_MCMETROLOGY_Initialize (
SYS_MODULE_INIT * init,
uint32_t resetCause
);SummaryInitializes the metrology driver according to the init parameter and the cause of the reset of the main processor.
DescriptionThis routine initializes the metrology driver making it ready for clients to open and use. The initialization data is specified by the init parameter. It is a single instance driver.
Note: This function is called by System Initialization when
program starts, this is, on power-up or after any reset. Depending on the reset
cause, the behaviour is different. When reset is due to Watchdog on Main
Processor, Coprocessor is not reset, allowing it to continue running
independently from the watchdog reset. Upon any other reset cause, the
Coprocessor is reset, but not its peripherals, this allows any previous
configuration from Main Processor to remain valid, as Coprocessor peripherals
can be used by Main Processor.
Parameters| Param | Description |
|---|---|
| init | Pointer to the init data structure containing any data necessary to initialize the driver. |
| resetCause | Reset cause of the main processor. |
If successful, returns a valid handle to a driver instance object. Otherwise, it returns SYS_MODULE_OBJ_INVALID.
ExampleSYS_MODULE_OBJ sysObjDrvMCMet;
extern uint8_t met_bin_start;
extern uint8_t met_bin_end;
/* Metrology Driver Initialization Data */
DRV_MCMETROLOGY_INIT drvMCMetrologyInitData = {
/* MET bin destination address */
.regBaseAddress = DRV_MCMETROLOGY_REG_BASE_ADDRESS,
/* MET Binary start address */
.binStartAddress = (uint32_t)&met_bin_start,
/* MET Binary end address */
.binEndAddress = (uint32_t)&met_bin_end,
};
sysObjDrvMet = DRV_METROLOGY_Initialize((SYS_MODULE_INIT *)&drvMetrologyInitData, RSTC_ResetCauseGet());RemarksThis routine must be called before any other DRV_MCMETROLOGY routine is called.