2.1.4.21 DRV_MCMETROLOGY_GetMeasureValue Function

C
float DRV_MCMETROLOGY_GetMeasureValue(DRV_MCMETROLOGY_MEASURE_TYPE type);
Summary

Gets the last value of the selected measurement type.

Description

Gets the last value of the selected measurement type on the selected power. Values are updated at the end of each integration period. For additional information about Measurement types, refer to the DRV_MCMETROLOGY_MEASURE_TYPE definition.

Parameters
ParamDescription
typeIndicate what type of measurement is obtained.
Returns

The value of the selected type.

Example
DRV_MCMETROLOGY_UpdateMeasurements();

app_metrologyData.queueFree = uxQueueSpacesAvailable(appEnergyQueueID);
if (app_metrologyData.queueFree)
{
    newMetrologyData.energy = DRV_MCMETROLOGY_GetEnergyValue(true);
    newMetrologyData.Pt = DRV_MCMETROLOGY_GetMeasureValue(MEASURE_PT);
    xQueueSend(appEnergyQueueID, &newMetrologyData, (TickType_t) 0);
}
else
{
    SYS_CMD_MESSAGE("ENERGY Queue is FULL!!!\n\r");
}
Remarks

None.