2.1.4.2 DRV_MCMETROLOGY_Reinitialize Function

C
SYS_MODULE_OBJ DRV_MCMETROLOGY_Reinitialize (
    SYS_MODULE_INIT * init
);
Summary

Re-initializes the metrology driver according to the init parameter.

Description

This routine re-initializes the metrology driver resetting the Coprocessor and its peripherals and re-loading the metrology library application on Core 1 from scratch. The initialization data is specified by the init parameter. It is a single instance driver.

Note: As described above, this routine resets the Coprocessor peripherals. User must be aware of this if Main Processor is using peripherals from Coprocessor, as they will require reconfiguration after reset.
Precondition

The low-level board initialization must have been completed and the module's initialization function must have been called before the system.

Parameters
ParamDescription
initPointer to the init data structure containing any data necessary to initialize the driver.
Returns

If successful, returns a valid handle to a driver instance object. Otherwise, it returns SYS_MODULE_OBJ_INVALID.

Example
SYS_MODULE_OBJ   sysObjDrvMet;

extern uint8_t met_bin_start;
extern uint8_t met_bin_end;

/* Metrology Driver Initialization Data */
DRV_MCMETROLOGY_INIT drvMCMetrologyInitData = {

    /* MET bin destination address */
    .regBaseAddress = DRV_MCMETROLOGY_REG_BASE_ADDRESS,

    /* MET Binary start address */
    .binStartAddress = (uint32_t)&met_bin_start,
    
    /* MET Binary end address */
    .binEndAddress = (uint32_t)&met_bin_end,
    
};

sysObjDrvMet = DRV_MCMETROLOGY_Initialize((SYS_MODULE_INIT *)&drvMCMetrologyInitData);
Remarks

None.