ZDO_ZdpReq Function
C
void ZDO_ZdpReq(ZDO_ZdpReq_t *zdpReq);Description
Sends a ZDP request
This function is used by an application to send a ZigBee Device Profile (ZDP) request. Request's type is determined by the argument's ZDO_ZdpReq_t-reqCluster field. Possible values are listed \ref ZdpClustersList "here". Specific request's parameters are set in the req.reqPayload field.
Response statuses: Accessed via the ZDO_ZdpRespFrame_t-status field of the ZDO_ZdpResp_t-respPayload field of the ZDO_ZdpReq_t-ZDO_ZdpResp callback's argument
All requests
-ZDO_SUCCESS_STATUS (0x00) - the request executed successfully \n -ZDO_FAIL_STATUS (0x07) - unknown error occured \n -ZDO_RESPONSE_WAIT_TIMEOUT_STATUS (0x02) - response has not been received
in required time. This status is not valid for the match descriptor request.
-ZDO_NOT_SUPPORTED_STATUS (0x84) - the requested feature is not
supported by the destination node
-ZDO_NOT_AUTHORIZED_STATUS (0x8D) - the node is not authorized to make such request \n\n
Match descriptor request
-ZDO_CMD_COMPLETED_STATUS (0x0D) - response timer has expired - not more responses
for the current request will be processed
Binding request
-ZDO_NO_ENTRY_STATUS (0x88) - unbinding request is unsuccessful, because the requested
entry has not been found in the binding table
-ZDO_TABLE_FULL_STATUS (0x8C) - the destination binding table is full -ZDO_INVALID_REQUEST_STATUS (0x80) - invalid parameters have been provided (endpoint ID is
out of range, incorrect destination addressing mode is used - APS_EXT_ADDRESS is expected, etc.)
Simple descriptor and complex descriptor requests
-ZDO_INVALID_EP_STATUS (0x82) - the specified endpoint has not been found on the
destination node
End device binding request
-ZDO_NOT_PERMITTED_STATUS (0x8B) - indicates that the coordinator has already
received end device binding requests from two other devices and cannot process one more request
Parameters
| Param | Description |
|---|---|
| zdpReq | Determines the parameters of the ZDP request |
Returns
None