ZDO_BindIndication Function
C
void ZDO_BindIndication(ZDO_BindInd_t *bindInd);Description
Indicates that a new binding has been added to the local binding table
The function must be implemented by the application (the body may be left empty). The function is called by the stack when a ZDP binding request initiated either by a remote device or by the local device is executed (a new binding entry is added).
When the APS_BindReq() function is called to add a new entry to the local binding table the indication function is not called.
Parameters
| Param | Description |
|---|---|
| bindInd | ZDO bind indication parameters structure pointer. For details go to ZDO_BindInd_t declaration. |
Returns
None