1.4.4.59 LUTwInterpolation_Q15 Function
fract_q15_t LUTwInterpolation_Q15( fract_q15_t x,
const fract_q15_t * pX_LUT_Vector,
const fract_q15_t * pY_LUT_Vector,
const uint16_t nLUTSize );Summary
Calculates calculates y = f(x) based on a lookup table with linear interpolation between table entries.
Description
Calculates calculates y = f(x) based on a lookup table with linear interpolation between table entries.
Preconditions
None.
Parameters
x Q15 value, independent variable
pX_LUT_Vector X column of LUT in Q15
pY_LUT_Vector Y column of LUT in Q15
nLutSize number of rows (entries) in the LUT
Returns
y = f(x) based on the LUT using linear interpolation between table entries.
Remarks
It is assumed that X LUT vector is in strictly monotonically increasing order.
That is: pX_LUT_Vector < pX_LUT_Vector for i = 0,1,...nLUTSize-2
Internal math is done in signed 32 integers and truncated to Q15.
If x <= pX_LUT_Vector then pY_LUT_Vector is returned.
if pX_LUT_Vector <= x then pY_LUT_Vector is returned.
Warning: It is strongly recommended that you test out the LUT and compare actual vs. desired values in Matlab/Octave or Excel! You may need to add additional rows where the interpolation does not produce the needed accuracy.
C
fract_q15_t LUTwInterpolation_Q15 (fract_q15_t x , const fract_q15_t * pX_LUT_Vector , const fract_q15_t * pY_LUT_Vector , const uint16_t nLUTSize );