4.8.4 Physical Layer Collision Avoidance (PLCA) Diagnostics
The PHY implements a number of features useful to the detection of PLCA misconfiguration on the network segment. These features include error status indications and event counters.
For revision C2 and earlier products, the PLCA error status indicators are located in the Status 1 (STS1) register. Each indication also has an associated interrupt mask bit in the Interrupt Mask 1 (IMSK1) register to enable an assertion of the interrupt on IRQ_N pin to the station host controller when the event is detected.
Revision D0 of the device implements the PLCA error status indicators in the OPEN Alliance standard PLCA Diagnostics (PLCA_DIAG) register. When one of these PLCA diagnostic bits is set, the PLCA Diagnostic (PLCADIAG) bit in the Status 1 (STS1 - Rev D0) register is set. The PLCA Diagnostic Mask (PLCADIAGM) bit in the Interrupt Mask 1 (IMSK1 - Rev D0) register may be written to ‘0’ to enable an assertion of the interrupt on IRQ_N pin to the station host controller when the PLCADIAG status bit is set.
Each node of a PLCA segment must be assigned a unique Local ID to properly avoid collisions. The device has the ability to detect that another node is assigned the same Local ID by detecting the reception of a packet from the network during its assigned transmit opportunity. When this condition occurs, the Receive in Transmit Opportunity (RXINTO) status bit is set. Additionally, should a collision be detected while the device is transmitting in its assigned transmit opportunity, the Transmit Collision (TXCOL) status bit will be set.
Multiple nodes configured and acting as PLCA Coordinators also cause problems. Multiple Coordinators on the mixing segment will each transmit a BEACON according to its own PLCA bus cycle and timing. The result is that each Coordinator will receive BEACONs that it did not transmit. When configured as a PLCA Coordinator, it will set the Unexpected BEACON Received (UNEXPB) status bit to indicate the presence of another Coordinator on the network segment.
The PLCA Coordinator must be configured with the correct number of nodes on the segment to permit the proper number of transmit opportunities per bus cycle. If the Coordinator is configured to allow for too few transmit opportunities between BEACONs, Follower nodes may not have access to their assigned transmit opportunity. When the device is operating as a PLCA Follower, if it detects a BEACON before its assigned transmit opportunity occurs then the BEACON Received Before Transmit Opportunity (BCNBFTO) status bit is set to indicate that the configured PLCA bus cycle is too small to allow the Follower to transmit.
When configured as a PLCA Follower, the PLCA Status (PST) bit in the PLCA Status (PLCA_STS) register will be set as long as BEACONs are regularly being received from a Coordinator. If BEACONs are not received by the device it will continue incrementing its transmit opportunity counter. When the transmit opportunity counter reaches the maximum count of 255, it will then stop incrementing and a 13 ms timer is started. If no BEACON is received after the timer expires, the PLCA Status bit will be cleared. When the PLCA Status bit is zero, the device will revert to CSMA/CD operation with PLCA deactivated. Once a BEACON is received the device will set the PLCA Status bit and return to normal PLCA operation. Refer to Clause 148 of the IEEE Std 802.3 specification for additional details. When the PLCA Status bit changes, the PLCA Status Changed (PSTC) bit in the Status 1 register is set and will assert the IRQ_N pin, if enabled in the Interrupt Mask 1 register.
The number of transmit opportunities in the PLCA bus cycle may be determined by reading the Maximum ID (MAXID) field of the PLCA Reconciliation Sublayer Status (PRSSTS) register. The MAXID field is updated at the end of each bus cycle. When read it will contain the number of transmit opportunities the PLCA coordinator allowed in the previous bus cycle.
Two event counters are implemented to aid the host controller in monitoring PLCA on the segment. These counters include a transmit opportunity counter and a BEACON counter. Each counter is enabled by setting the corresponding enable bit in the Counter Control (CTRCTRL) register. Writing a ‘1’ to the Transmit Opportunity Counter Enable (TOCTRE) bit enables the transmit opportunity counter. The BEACON Counter Enable (BCNCTRE) bit enables the BEACON counter when set.
When enabled, the Transmit Opportunity Count High/Low (TOCNTH/TOCNTL) registers will contain the number of transmit opportunities the local PHY could have used to transmit since the last read. By polling the counter, the host controller can monitor that PLCA is active and that the PHY can transmit packets when needed.
Similarly, the BEACON Count High/Low (BCNCNTH/BCNCNTL) register contains the number of received BEACONs since the last read. The host controller can poll this counter to monitor the health of the PLCA Coordinator.