2.2.4.2.3 Memory Initialization at Power-Up

In the Memory Initialization tab, the user can initialize RAM at power-up. μSRAM can be initialized during device power-up and functional simulation as described in Memory Initialization at Power-Up of Dual-Port Large SRAM Configurator. The following figure shows the μSRAM IP memory initialization.

Figure 2-32. MicroSRAM Configurator: Memory Initialization

The Reset All Values option resets all the data values. This option is enabled when the RAM Content Editor check box is selected.