21.10.22 set_client
(Ask a Question)Description
Use the following Tcl command to specify the client that will be added to the SPI
                Flash memory configuration file along with the configure_spiflash
                command.
set_client -client_name {client name} \
           -client_type {FILE_SPI | FILE_SPI_GOLDEN | FILE_SPI_UPDATE | FILE_DATA_STORAGE_INTELHEX} \
           -content_type {MEMORY_FILE | STATIC_FILL} \
           -content_file {} \
           -start_address {} \
           -client_size {} \
           -program {0|1}
            Use the following Tcl command to specify the client that will be added to the fabric
                RAM configuration file along with the configure_ram command.
set_client \
   -logical_instance_name  {RAM user defined instance name}  \
   -storage_type { Initialization client storage type}  \
   -content_type { NO_CONTENT | MEMORY_FILE } \
   -memory_file_format { Intel-Hex | Motorola-S | Simple-Hex | Microsemi-Binary}  \
   -memory_file {path}
        Arguments
| Parameter | Type | Description | 
|---|---|---|
| client_name | string | The name of the client. Maximum of 32 characters, letters or numbers or “-“ or “_”. | 
| client_type | string | The -client_type can be FILE_SPI, FILE_SPI_GOLDEN, FILE_SPI_UPDATE orFILE_DATA_STORAGE_INTELHEX. 
  | 
| content_type | string | Specifies the type of memory content: 
  | 
| content_file | string | Absolute or relative path to the content memory file. | 
| start_address | integer | The client start address. Note that some space is reserved for the SPI Flash Memory directory. This is a decimal value of bytes. | 
| client_size | integer | Client’s size in bytes. If a content file is specified, the size must be equal to or larger than the file size. This is a decimal value. | 
| program | boolean | Only program | 1 is supported in this release. | 
| logical_instance_name | string | Specifies the name for the user defined memory instance. | 
| storage_type | string | Specifies storage type to initialize RAM: 
  | 
| memory_file_format | string | Specifies the memory file format:
  | 
| memory_file | string | Specifies the absolute or relative path of the memory file. | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
| None | None | 
Supported Families
| PolarFire® | 
| PolarFire SoC | 
Example
The following examples show the set_client Tcl command for SPI
                Flash.
set_client -client_name {golden} \
           -client_type {FILE_SPI_GOLDEN} \
           -content_type {MEMORY_FILE} \
           -content_file {E:\top_design_ver_1.spi} \
           -start_address {1024} \
           -client_size {9508587} \
           -program {1}
            set_client -client_name {cl1} \
           -client_type {FILE_DATA_STORAGE_INTELHEX} \
           -content_type {STATIC_FILL} \
           -content_file {} \
           -start_address {1024} \
           -client_size {100} \
           -program {1}
            The following examples show the set_client Tcl command for the
                fabric RAM configuration file.
set_client \
   -logical_instance_name  {PF_TPSRAM_C0_0/PF_TPSRAM_C0_0}  \
   -storage_type {SNVM}  \
   -content_type {MEMORY_FILE}  \
   -memory_file_format {}  \
   -memory_file {Y:/DP_mem/DPRAM_1k_20/hexmod.hex}