21.10.15 set_auto_update_mode
(Ask a Question)Description
This Tcl command enables or disables auto update. This command is added to the spiflash.cfg file that is given as the parameter to the configure_spiflash command.
set_auto_update_mode {0|1}Arguments
| Parameter | Type | Description | 
|---|---|---|
| None | boolean | If set_auto_update_mode is 0, auto update is disabled. If set_auto_update_mode is 1, auto update is enabled. | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
| None | None | 
Supported Families
| PolarFire® | 
| PolarFire SoC | 
Example
This example sets auto update disabled.
set_auto_update_mode {0}