21.10.20 set_plain_text_client
(Ask a Question)Description
This Tcl command is added to the sNVM.cfg file that is given as the parameter to
                the configure_snvm command.
set_plain_text_client -client_name {name} \
                      -number_of_bytes {number} \
                      -content_type {MEMORY_FILE | STATIC_FILL} \
                      -content_file_format {Microchip-Binary 8/16/32 bit} \
                      -content_file {path} \
                      -start_page {number} \
                      -use_for_simulation {0} \
                      -reprogram {0 | 1} \
                      -use_as_rom {0 | 1}Arguments
| Parameter | Type | Description | 
|---|---|---|
| client_name | string | Specifies the name of the client. Needs to start with an alphabetic letter. Underscores and numerals are allowed at all positions other than the first. | 
| number_of_bytes | integer | The size of the client specified in bytes. | 
| content_type | string | Source of data for the client. This can either be a memory file, or all zeros. Allowed values are MEMORY_FILE or STATIC_FILL | 
| content_file_format | string | Only ‘Microchip-Binary 8/16/32 bit’ is supported at this time. | 
| content_file | string | Path of the memory file. This can be absolute, or relative to the project. | 
| start_page | integer | The page number in sNVM where data for this client will be placed. | 
| use_for_simulation | boolean | Only value 0 is allowed. | 
| reprogram | boolean | Specifies whether the client will be programmed into the final design or not. Possible values are 0 or 1. | 
| use_as_rom | boolean | Specifies whether the client will allow only reads, or both read and writes. Possible values are 0 or 1. | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
| None | None | 
Supported Families
| PolarFire® | 
| PolarFire SoC | 
Example
This example sets plain_tets client with the following parameter values.
set_plain_text_client -client_name {a} \
                      -number_of_bytes 12 \
                      -content_type {MEMORY_FILE} \
                      -content_file_format {Microchip-Binary 8/16/32 bit} \
                      -content_file {} \
                      -start_page 1 \
                      -use_for_simulation 0 \
                      -reprogram 1 \
                      -use_as_rom 0See Also
- set_cipher_text_auth_client
 - set_usk_client