Description
            
            This Tcl command appears in the fabric RAM configuration file when the Fabric RAM is
                modified to initialize memory.
            modified_client \
   -logical_instance_name  { RAM user defined instance name }  \
   -storage_type { Initialization client storage type }  \
   -content_type { NO_CONTENT | MEMORY_FILE }  \
   -memory_file_format { Intel-Hex | Motorola-S | Simple-Hex | Microsemi-Binary }  \
   -memory_file { path }
        Arguments
| Parameter | Type | Description | 
|---|
| logical_instance_name | string | Specifies the name of the user defined memory instance. | 
| storage_type | string | Specifies storage type to initialize RAM:  | 
| content_type | string | Specifies the type of memory content: - MEMORY_FILE -
                                        content_file parameter must be specified.
 - NO_CONTENT -
                                        no content memory file.
 
  | 
| memory_file_format | string | Specifies the memory file format:- Intel-Hex
 - Motorola-S
 - Simple-Hex
 - Microchip-Binary
 
  | 
| memory_file | string | Specifies the absolute or relative path of the memory
                                file. | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | None | 
Example
The following example show the modified_client Tcl command.
modified_client \
   -logical_instance_name  {PF_TPSRAM_C0_0/PF_TPSRAM_C0_0}  \
   -storage_type {SNVM}  \
   -content_type {MEMORY_FILE}  \
   -memory_file_format {Intel-Hex}  \
   -memory_file {Y:/TP_mem/TPRAM_1024_40lp/mem_files/hex .hex}