21.10.16 set_manufacturer
(Ask a Question)Description
This command specifies the manufacturer for the SPI Flash device.
set_manufacturer {MICRON | SPANSION | Macronix | Winbond }Arguments
| Parameter | Type | Description | 
|---|---|---|
| None | string | The value for the set_manufacturer command must be one of the following: 
  | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
| None | None | 
Supported Families
| PolarFire® | 
| PolarFire SoC | 
Example
This example sets the manufacturer {MICRON}.
set_manufacturer {MICRON}