Description
This Tcl command sets a BSDL file to a non-Microchip device in the chain. Chain programming mode
                must have been set. The device must be a non-Microchip device.
set_bsdl_file -name {device name} -file {path to the BSDL file}
Arguments
| Parameter | Type | Description | 
|---|
| name | string | Specifies the device name. | 
| file | string | Specifies the BSDL file. | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Parameter 'file' has illegal value. | 
| None | Required parameter 'file' is missing. | 
| None | Parameter 'name' has illegal value. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'set_bsdl_file -name "name" -file "file"'. | 
Supported Families
            
            | Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
 
        Example
The following example sets the BSDL file ./src/top.bsd to the device
                'MyDevice':
set_bsdl_file -name {MyDevice} -file {./src/top.bsd}