Description
This Tcl command automatically starts chain construction for the specified programmer.
construct_chain_automatically -name {name}
Arguments
| Parameter | Type | Description | 
|---|
| name | string | Specifies the programmer(s) name(s). You can repeat this argument to specify multiple programmers names. | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Required parameter 'name' is missing. | 
| None | Parameter 'name' is missing or has invalid value. | 
| None | Parameter 'name' has illegal value. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'construct_chain_automatically [-name "name"]+'. | 
Supported Families
            
            | Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
 
        Example
For a single programmer:
construct_chain_automatically -name {E2004NSXB1}
See Also
- scan_chain_prg
 - enable_device
 - set_debug_programmer
 - set_device_name
 - set_programming_file
 - set_programming_action
 - run_selected_actions