Description
This Tcl command removes settings for non-Microchip or non-Actel device from the device
                database.
remove_non_actel_device_from_database [-name {device name}]
Arguments
| Parameter | Type | Description | 
|---|
| name | string | Specifies the non-Actel or non-Microchip device name to be removed from the database. You can
                                repeat this argument for multiple devices. | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Required parameter 'name' is missing. | 
| None | The device 'device_name' does not exist in the database. | 
| None | Parameter 'name' is missing or has invalid value. | 
| None | Parameter 'name' has illegal value. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'remove_non_actel_device_from_database [-name "name"]+'. | 
Supported Families
            
            | Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
 
        Example
The following example removes the "F1502AS" device from the database:
remove_non_actel_device_from_database -name {F1502AS}
See Also
- add_non_actel_device_to_database