Description
This Tcl command changes the family of a Microchip device in the chain. The device must be a
                Microchip device.
set_device_type [-name {device name}] -type {type}
Arguments
| Parameter | Type | Description | 
|---|
| name | string | Identifies the name of the device you want to change. This parameter is optional. | 
| type | string | Specifies the device family. This parameter is mandatory. | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Required parameter 'type' is missing. | 
| None | Parameter 'type' has illegal value. | 
| None | Parameter 'name' has illegal value. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'set_device_type [-name "name"] -type "type"'. | 
Supported Families
            
            | Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
 
        Example
The following example sets the device 'MyDevice' to the type MPF324.
set_device_type -name {MyDevice} -type {MPF324}