Description
This Tcl command changes the user name of a device in the chain. Chain programming mode must be set.
set_device_name -name {name} -new_name {new_name}
Arguments
| Parameter | Type | Description | 
|---|
| name | string | Identifies the old device name. This parameter is mandatory. | 
| new_name | string | Specifies the new device name. This parameter is mandatory. | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Required parameter 'name' is missing. | 
| None | Required parameter 'new_name' is missing. | 
| None | The device with name 'device_name' doesn't exist. | 
| None | Parameter 'name' has illegal value. | 
| None | Parameter 'new_name' has illegal value. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'set_device_name -name "name" -new_name "new_name"'. | 
Supported Families
            
            | Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
 
        Example
The following example changes the user name of the device from 'MyDevice1' to 'MyDevice2':
set_device_name -name {MyDevice1} -new_name {MyDevice2}