Description
This Tcl command enables or disables a device in the chain (if the device is disabled, it is
                bypassed). Chain programming mode must be set. The device must be a Microchip
                device.
enable_device -name {device name} -enable {TRUE | FALSE}
Arguments
| Parameter | Type | Description | 
|---|
| name | string | Specifies your device name. This parameter is mandatory. | 
| enable | boolean | Specifies whether the device is to be enabled or disabled. If you specify multiple devices, this argument applies to all specified devices. Specify 1 or "TRUE" to enable device, specify 0 or "FALSE" to enable device. | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Required parameter 'name' is missing. | 
| None | Required parameter 'enable' is missing. | 
| None | The device with name 'MyDevice1' doesn't exist | 
| None | enable: Invalid argument value: '' (expecting TRUE, 1, true, FALSE, 0 or false). | 
| None | Parameter 'enable' has illegal value. | 
| None | Parameter 'name' has illegal value. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'enable_device -name "name" -enable "TRUE | FALSE"'. | 
Supported Families
            
            | Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
 
        Example
The following example disables the device 'MyDevice' in the chain.
enable_device -name {MyDevice} -enable {FALSE}