Network ARP Inspection Dynamic Table Configuration
Entries in the Dynamic ARP Inspection table are shown on the Dynamic ARP Inspection Table page. The Dynamic ARP Inspection table contains up to 256 entries, and is sorted in the following order:
- Port
- VLAN ID
- MAC address
- IP address
All Dynamic ARP Inspection Table dynamic entries learn from DHCP Snooping.
The page has the following parameters:
- Port: Switch Port Number for which the entries are displayed
- VLAN ID: VLAN ID in which the ARP traffic is permitted
- MAC Address: User MAC address of the entry
- IP Address: User IP address of the entry
- Translate to Static: Select the checkbox to translate the entry to static entry