GATTS_Service_T
C
typedef struct GATTS_Service_T
{
struct GATTS_Service_T *p_next;
GATTS_Attribute_T *p_attrList;
GATTS_CccdSetting_T const *p_cccdSetting;
uint16_t startHandle;
uint16_t endHandle;
uint8_t cccdNumber;
} GATTS_Service_T;Description
Structure for a GATT service with its attributes and handles.
Field Documentation
| Field | Description |
|---|---|
| p_next | Pointer to the next service in a linked list. For internal chaining of services. |
| p_attrList | Pointer to the array of attributes within this service. See GATTS_Attribute_T. |
| p_cccdSetting | Pointer to the CCCD settings for the service. May be NULL if not used. See GATTS_CccdSetting_T. |
| startHandle | Handle of the first attribute in the service. |
| endHandle | Handle of the last attribute in the service. |
| cccdNumber | Count of Client Characteristic Configuration Descriptors (CCCDs) in the service. |