3.6.4.20 MCP25625 Click Example on SAM E51 Curiosity Nano Evaluation Kit
Description
This example demonstrates the transmitting and receiving of CAN data using the MCP25625 CAN click board and displays the transmit/receive CAN message on a serial terminal on SAM E51 Curiosity Nano Evaluation Kit using the MCP25625 Click board.
Modules/Technology Used
- Peripheral Modules:
- PORT
- SERCOM (SPI)
- SYSTICK
Hardware Used
- SAM E51 Curiosity Nano Evaluation Kit - 2 Units
- Curiosity Nano Base for Click Boards - 2 Units
-
MikroElektronika MCP25625 Click - 2 Units
Note: One of the two hardware setups is required for the CAN message transmission (Setup-1) and the other for reception(Setup-2). Parallelly both the setups demonstrate CAN data transmission and reception.
Software/Tools Used
This project has been verified to work with the following versions of software tools:
Refer Project Manifest present in harmony-manifest-success.yml under the project folder firmware/src/config/sam_e51_cnano.
- Refer the Release Notes to know the MPLAB X IDE and MCC Plugin version.
Because Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected. It is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).
Setup
- Connect the SAM E51 Curiosity Nano Evaluation Kit to the Host PC as a USB Device through a Type-A male to micro-B USB cable connected to Micro-B USB (Debug USB) port.
- Mount MikroElektronika MCP25625 Click over mikroBUS socket #1 on the SAM E51 Curiosity Nano Evaluation Kit (Setup-1).
- Repeat the above steps with the other hardware units (Setup-2).
- Short the CANH and CANL lines of one
DB9 connector with the CANH and CANL line of another DB9 connector using jumper wires
as shown below image.
- CANH - Pin 7 of the DB9 connector
- CANL - Pin 2 of the DB9 connector
Programming Hex File
The pre-built hex file can be programmed by following the below steps.
- Open MPLAB X IDE
- Close all existing projects in IDE, if any project is opened.
- Go to File -> Import -> Hex/ELF File.
- In the Import Image File
window,
- Create Prebuilt Project,
- Click the Browse button to select the prebuilt hex file.
- Select Device as ATSAME51J20A.
- Ensure the proper tool is selected under Hardware Tool and click on Next button.
- Select Project Name and Folder,
- Select appropriate project name and folder and click on Finish button
- Create Prebuilt Project,
- In MPLAB X IDE, click on Make and Program Device button to program the device.
- Follow the steps in Running the Demo section below.
Programming/Debugging Application Project
- Open the project (apps/sam_e51_cnano/same51n_mikroe_click/mcp25625/firmware/sam_e51_cnano.X) in MPLAB X IDE
- Ensure SAM E51 Curiosity Nano Evaluation Kit is selected as hardware tool to program/debug the application
- Build the code and program the device by clicking on the Make and Program button in MPLAB X IDE tool bar
- Follow the steps in Running the Demo section below
Running the Demo
- Open the Tera Term terminal application on the PC (from the Windows Start menu by pressing the Start button).
- Set the baud rate to 115200.
- Repeat the above two steps for the
second hardware setup (Setup-2).


- Enter a character 'a' on one Tera terminal application to initiate the CAN Message Transmit.
- Enter a character 'b' on
another Tera terminal application to wait for the CAN Message Receive.


- In both the Tera terminal windows, the user will see the CAN message transmission and reception continuously.
Instructions to Add MCP25625 Functionality to the Application
The user could use this demonstration as an example to add MCP25625 functionality to the MPLAB Harmony v3-based application. Follow the below steps.
- If the user has not downloaded the MCP25625 demo yet Click Here to download, otherwise go to the next step.
- Unzip the downloaded .zip file.
- From the unzipped folder mcp25625/firmware/src, copy the folder click_routines to the folder firmware/src under the MPLAB Harmony v3 application project.
- Open MPLAB X IDE.
- Open the application project.
- In the project explorer, right click on
folder Header Files and add a sub folder click_routines by selecting
Add Existing Items from Folders...

- Click on Add Folder... button.

- Select the click_routines folder and select Files of Types as Header
Files.

- Click on Add button to add the selected folder.

- The MCP25625 click example header files gets added to the project.

- In the project explorer, right click on folder Source Files and add a sub
folder click_routines by selecting Add Existing Items from Folders...

- Click on Add Folder... button.

- Select the click_routines folder and select Files of Types as Source
Files.

- Click on Add button to add the selected folder.

- The MCP25625 click example source files gets added to the project.

- The MCP25625 click example uses the SPI peripheral. The configuration of this
peripheral for the application depends on the 32-bit MCU and development board the user
is using.
- Configure SPI:
- Add the SPI peripheral block to the MCC project graph.
- Configure SPI Pins using MCC
Pin configuration Window.The SPI configuration depends on:
- 32-bit MCU
- 32-bit MCU development board
- The socket on which the
user has mounted the MCP25625 click board
Example: The MCP25625 click example on SAM E51 Curiosity Nano Evaluation Kit uses mikroBUS socket #1 on the Curiosity Nano Base for Click boards to mount the MCP25625 click board. The SPI lines from MCU coming to this socket are from the SERCOM1 peripheral on the MCU.
Figure 3-67. MCC Project Graph - SPI Configuration Figure 3-68. MCC Pin Configurator - SPI Pin Configuration 
- Configure PORT Pins:
- The MCP25625 click needs three
additional pins for configuration and data exchange. These parent:
- Standby pin
- Reset pin
- Configure PORT pins needed by
MCP25625 click in the MCC Pin Configurator.The PORT pin configuration depends on:
- 32-bit MCU
- 32-bit MCU development board
- The socket on which the
user has mounted the MCP25625 click board
Example: The PORT pin configuration for the MCP25625 click example on SAM E51 Curiosity Nano Evaluation Kit is below.
Figure 3-69. MCC Pin Configurator - PORT Pin Configuration
- The MCP25625 click needs three
additional pins for configuration and data exchange. These parent:
- Map Generic Macros:
- After generating the project, following the above configuration, map the generic macros used in the click routines to the Harmony PLIB APIs of the 32-bit MCU the project is running on.
- The generic macros should be
mapped in the header file click_interface.h.

Example: The MCP25625 click routines for the example on SAM E51 Curiosity Nano Evaluation Kit uses the following Harmony PLIB APIs.
The click_routines folder contain an example C source file mcp25625_example.c. The user could use mcp25625_example.c as a reference to add MCP25625 functionality to the application.
- Configure SPI:
Comments
- Reference Training Module:
- This application demo builds and
works out of box by following the instructions above in Running the Demo
section. If the user needs to enhance/customize this application demo, should use the
MPLAB Harmony v3 Software framework. Refer links below to setup and build the
applications using MPLAB Harmony.
- How to Setup MPLAB Harmony v3 Software Development Framework (DS90003232).
- How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project (DS90003253).
- Video - How to Set up the Tools Required to Get Started with MPLAB® Harmony v3 and MCC
- Create a new MPLAB Harmony v3 project using MCC
- Update and Configure an Existing MHC-based MPLAB Harmony v3 Project to MCC-based Project