3.6.4.21 Eink E-Paper Display 2,9" 296x128 Dots Display Example on SAM E51 Curiosity Nano Evaluation Kit
Description
This example demonstrates the display capability of Eink E-Paper display 2,9" 296x128 dots display board on SAM E51 Curiosity Nano Evaluation Kit.
Modules/Technology Used
- Peripheral Modules:
- SYSTICK
- GPIO
- SERCOM (SPI)
Hardware Used
Software/Tools Used
This project has been verified to work with the following versions of software tools:
Refer Project Manifest present in harmony-manifest-success.yml under the project folder firmware/src/config/sam_e51_cnano.
- Refer the Release Notes to know the MPLAB X IDE and MCC Plugin version.
Because Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected. It is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).
Setup
- Connect the SAM E51 Curiosity Nano
Evaluation Kit to the Host PC as a USB Device through a Type-A male to micro-B USB
cable connected to Micro-B USB (Debug USB) port.
Programming Hex File
The pre-built hex file can be programmed by following the below steps.
- Open MPLAB X IDE.
- Close all existing projects in IDE, if any project is opened.
- Go to File -> Import -> Hex/ELF File.
- In the Import Image File
window,
- Create Prebuilt Project,
- Click the Browse button to select the prebuilt hex file.
- Select Device as ATSAME51J20A.
- Ensure the proper tool is selected under Hardware Tool and click on Next button.
- Select Project Name and Folder,
- Select appropriate project name and folder and click on Finish button
- Create Prebuilt Project,
- In MPLAB X IDE, click on Make and Program Device button to program the device.
- Follow the steps in Running the Demo section below.
Programming/Debugging Application Project
- Open the project (eink_epaper_2_9_296_128/firmware/sam_e51_cnano.X) in MPLAB X IDE
- Ensure SAM E51 Curiosity Nano is selected as hardware tool to program/debug the application
- Build the code and program the device by clicking on the Make and Program Device button in MPLAB X IDE tool bar
- Follow the steps in Running the Demo section below
Running the Demo
- After power up, when the demo is
running, the Eink E-Paper display 2,9" 296x128 dots display shows as below.
Instructions to Add Eink E-Paper Display 2,9" 296x128 Dots Display Functionality to the Application
The user could use this demonstration as an example to add Eink E-Paper display 2,9" 296x128 dots display functionality to the MPLAB Harmony v3 based application. Follow the below steps.
- If the user has not downloaded the Eink E-Paper display 2,9" 296x128 dots display demo yet Click Here to download, otherwise go to next step.
- Unzip the downloaded .zip file.
- From the unzipped folder eink_epaper_2_9_296_128/firmware/src, copy the folder click_routines to the folder firmware/src under the MPLAB Harmony v3 application project.
- Open MPLAB X ID.E
- Open the application project.
- In the project explorer, right click on folder Header Files and add a sub
folder click_routines by selecting Add Existing Items from Folders...

- Click on Add Folder... button.

- Select the click_routines folder and select Files of Types as Header
Files.

- Click on Add button to add the selected folder.

- The eink_epaper_2_9_296_128 display example header files gets added to the
project.

- In the project explorer, right click on folder Source Files and add a sub
folder click_routines by selecting Add Existing Items from Folders...

- Click on Add Folder... button.

- Select the click_routines folder and select Files of Types as Source
Files.

- Click on Add button to add the selected folder.

- The eink_epaper_2_9_296_128 display example source files gets added to the
project.

- The eink_epaper_2_9_296_128 display example uses the SPI, Timer
peripherals and PORT pins . The configuration of these peripherals for the
application depends on the 32-bit MCU and development board the user is using.
- Configure SPI:
- Add the SPI peripheral block to the MCC project graph.
- Configure SPI Pins using MCC
Pin configuration Window.The SPI configuration depends on:
- 32-bit MCU
- 32-bit MCU development board
- The socket on which the
user has mounted the Eink E-Paper display 2,9" 296x128 dots click
board
Example: The Eink E-Paper display 2,9" 296x128 dots example on SAM E51 Curiosity Nano Evaluation Kit uses mikroBUS socket #1 on the Curiosity Nano Base for Click boards to mount the Eink Click board. The SPI lines from MCU coming to this socket are from the SERCOM1 peripheral on the MCU.
Figure 3-70. MCC Project Graph - SPI Configuration 
Figure 3-71. MCC Pin Configurator - SPI Pin Configuration 
- Configure Timer:
- Configure Timer peripheral
block in the MCC project graph.The Timer configuration depends on:
- 32-bit MCU
Example: The Eink E-Paper display 2,9" 296x128 dots display example on SAM E51 Curiosity Nano Evaluation Kit uses SysTick timer module on the MCU to implement the time requirement of Eink E-Paper display 2,9" 296x128 dots click routines.
Figure 3-72. MCC Project Graph - SysTick Configuration 
- 32-bit MCU
- Configure Timer peripheral
block in the MCC project graph.
- Configure PORT Pins:
- The Eink E-Paper display 2,9"
296x128 dots needs three additional pins for configuration and data exchange.
These parent:
- Data/Config pin
- Busy indicator pin
- Reset pin
- Configure PORT pins needed by
Eink E-Paper display 2,9" 296x128 dots in the MCC Pin Configurator.The PORT pin configuration depends on:
- 32-bit MCU
- 32-bit MCU development board
- The socket on which the
user has mounted the Eink click board
Example: The PORT pin configuration for the Eink E-Paper display 2,9" 296x128 dots example on SAM E51 Curiosity Nano Evaluation Kit is below.
Figure 3-73. MCC Pin Configurator - PORT Pin Configuration 
- The Eink E-Paper display 2,9"
296x128 dots needs three additional pins for configuration and data exchange.
These parent:
- Map Generic Macros:
- After generating the project, following the above configuration, map the generic macros used in the click routines to the Harmony PLIB APIs of the 32-bit MCU the project is running on.
- The generic macros should be
mapped in the header file click_interface.h.

Example: The Eink E-Paper display 2,9" 296x128 dots display routines for the example on SAM E51 Curiosity Nano Evaluation Kit uses the following Harmony PLIB APIs.
The click_routines folder contain an example C source file eink_epaper_2_9_296_128_example.c. The user could use eink_epaper_2_9_296_128_example.c as a reference to add Eink E-Paper display 2,9" 296x128 dots display functionality to the application.
- Configure SPI:
Comments
- Reference Training Module:
- This application demo builds and
works out of box by following the instructions above in Running the Demo
section. If the user needs to enhance/customize this application demo, should use the
MPLAB Harmony v3 Software framework. Refer links below to setup and build the
applications using MPLAB Harmony.
- How to Setup MPLAB Harmony v3 Software Development Framework (DS90003232).
- How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project (DS90003253).
- Video - How to Set up the Tools Required to Get Started with MPLAB® Harmony v3 and MCC
- Create a new MPLAB Harmony v3 project using MCC
- Update and Configure an Existing MHC-based MPLAB Harmony v3 Project to MCC-based Project