This example demonstrates the reading of temperature and displays it on a serial terminal
on SAM E51 Curiosity Nano Evaluation Kit using I/O1 Xplained Pro Extension Kit connected
to XPRO-ADAPTER Click board.
This project has been verified to work with the following versions of software tools:
Refer Project Manifest present in
harmony-manifest-success.yml under the project folder
firmware/src/config/sam_e51_cnano.
Refer the Release Notes to know the
MPLAB X IDE and MCC Plugin version.
Any Serial Terminal application, such
as Tera Term terminal application.
Because Microchip regularly updates tools, occasionally issue(s) could be discovered
while using the newer versions of the tools. If the project does not seem to work and
version incompatibility is suspected. It is recommended to double-check and use the same
versions that the project was tested with. To download original version of MPLAB Harmony
v3 packages, refer to document How to Use the MPLAB Harmony v3 Project Manifest Feature
(DS90003305).
Setup
Connect the SAM E51 Curiosity Nano
Evaluation Kit to the Host PC as a USB Device through a Type-A male to micro-B USB
cable connected to Micro-B USB (Debug USB) port.
Insert XPRO-ADAPTER
Click to mikroBUS socket #1 on the Curiosity Nano Base for Click boards as
shown in the following figure.
Programming Hex File
The pre-built hex file can be programmed by following the below steps.
Steps to program the hex file:
Open MPLAB X IDE.
Close all existing projects in IDE,
if any project is opened.
Go to File -> Import ->
Hex/ELF File.
In the Import Image File
window,
Create Prebuilt Project,
Click the Browse
button to select the prebuilt hex file.
Select Device as
ATSAME51J20A.
Ensure the proper tool is
selected under Hardware Tool and click on Next button.
Select Project Name and Folder,
Select appropriate project
name and folder and click on Finish button
In MPLAB X IDE, click on Make and
Program Device button to program the device.
Follow the steps in Running the
Demo section below.
Programming/Debugging Application
Project
Open the project
(sam_e51_cnano/same51n_mikroe_click/xpro_adapter/firmware/sam_e51_cnano.X) in MPLAB X
IDE
Ensure SAM E51 Curiosity Nano
is selected as hardware tool to program/debug the application
Build the code and program the device
by clicking on the Make and Program Device button in MPLAB X IDE tool bar
Follow the steps in Running the
Demo section below
Running the Demo
Open the Tera Term terminal application
on the PC (from the Windows Start menu by pressing the Start button).
Set the baud rate to 115200.
For every switch press, the SAM E51
Curiosity Nano Evaluation Kit to prints the temperature.
Instructions to Add XPRO Adapter
Functionality to the Application
The user could use this demonstration as an example to add XPRO Adapter functionality to
the MPLAB Harmony v3 based application. Follow the below steps.
If the user has not downloaded the XPRO
Adapter demo yet Click Here to download, otherwise go to next step.
Unzip the downloaded .zip file.
From the unzipped folder
xpro_adapter/firmware/src, copy the folder click_routines to the folder
firmware/src under the MPLAB Harmony v3 application project.
Open MPLAB X IDE.
Open the application project.
In the project explorer, right click on
folder Header Files and add a sub folder click_routines by selecting
Add Existing Items from Folders...
Click on Add Folder... button.
Select the click_routines folder and select Files of Types as Header
Files.
Click on Add button to add the selected folder.
The XPRO Adapter click example header files gets added to the project.
In the project explorer, Right click on folder Source Files and add a sub
folder click_routines by selecting Add Existing Items from Folders...
Click on Add Folder... button.
Select the click_routines folder and select Files of Types as Source
Files.
Click on Add button to add the selected folder.
The XPRO Adapter click example source files gets added to the project.
The XPRO Adapter click example uses the
I2C peripheral. The configuration of this peripheral for the
application depends on the 32-bit MCU and development board the user is using.
Configure I2C:
Add the I2C
peripheral block to the MCC project graph.
Configure I2C Pins
using MCC Pin configuration Window.
The I2C configuration depends
on:
32-bit MCU
32-bit MCU development
board
The socket on which the
user has mounted the XPRO Adapter click board
Example: The XPRO
Adapter click example on SAM E51 Curiosity Nano Evaluation Kit uses
mikroBUS socket #1 on the Curiosity Nano Base for Click boards to
mount the XPRO Adapter click board. The I2C lines from MCU
coming to this socket are from the SERCOM2 peripheral on the
MCU.
After generating the project,
following the above configuration, map the generic macros used in the click
routines to the Harmony PLIB APIs of the 32-bit MCU the project is running
on.
The generic macros should be
mapped in the header file click_interface.h.
Example: The XPRO Adapter click routines for the example on SAM E51
Curiosity Nano Evaluation Kit uses the following Harmony PLIB APIs.
The click_routines folder contain an example C source file
xpro_adapter_example.c. The user could use xpro_adapter_example.c as a
reference to add XPRO Adapter functionality in the application.
This application demo builds and
works out of box by following the instructions above in Running the Demo
section. If the user needs to enhance/customize this application demo, should use the
MPLAB Harmony v3 Software framework. Refer links below to setup and build the
applications using MPLAB Harmony.