3.6.4.4 LED DRIVER 3 Click Example on SAM E51 Curiosity Nano Evaluation Kit
Description
This example demonstrates RGB color (Red/Green/Blue) one by one with a 500ms delay on the LED Driver 3 click board when the switch is pressed on the SAM E51 Curiosity Nano Evaluation Kit.
Modules/Technology Used
- Peripheral Modules:
- EIC
- SYSTICK
- GPIO
- SERCOM (I2C)
- SERCOM (USART)
Hardware Used
Software/Tools Used
This project has been verified to work with the following versions of software tools:
Refer Project Manifest present in harmony-manifest-success.yml under the project folder firmware/src/config/sam_e51_cnano.
- Refer the Release Notes to know the MPLAB X IDE and MCC Plugin version.
- Any Serial Terminal application, such as Tera Term terminal application.
Because Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected. It is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).
Setup
- Mount SAM E51 Curiosity Nano Evaluation Kit on "CNANO56_HOST_CONN"(U3) connector of Curiosity Nano Base board.
- Mount LED Driver 3 Click board on mikroBUS click 1 connector of Curiosity Nano Base board.
- Connect the SAM E51 Curiosity Nano
Evaluation Kit to the Host PC as a USB Device through a Type-A male to micro-B USB
cable connected to Micro-B USB (Debug USB) port.
Programming Hex File
The pre-built hex file can be programmed by following the below steps.
- Open MPLAB X IDE
- Close all existing projects in IDE, if any project is opened.
- Go to File -> Import -> Hex/ELF File.
- In the Import Image File
window,
- Create Prebuilt Project,
- Click the Browse button to select the prebuilt hex file.
- Select Device as ATSAME51J20A.
- Ensure the proper tool is selected under Hardware Tool and click on Next button.
- Select Project Name and Folder,
- Select appropriate project name and folder and click on Finish button
- Create Prebuilt Project,
- In MPLAB X IDE, click on Make and Program Device button to program the device.
- Follow the steps in Running the Demo section below.
Programming/Debugging Application Project
- Open the project (leddriver3/firmware/sam_e51_cnano.X) in MPLAB X IDE
- Ensure PKOB nano is selected as hardware tool to program/debug the application
- Build the code and program the device by clicking on the Make and Program button in MPLAB X IDE tool bar
- Follow the steps in Running the Demo section below
Running the Demo:
- Open the Tera Term terminal application on the PC (from the Windows Start menu by pressing the Start button).
- Set the baud rate to 115200.
- Press the switch SW0 on the SAM E51 Curiosity Nano Evaluation Kit to display the RGB color (Red/Green/Blue) one by one with 500ms delay on LED Driver 3 click board.
- For every switch press, the SAM E51 Curiosity Nano Evaluation Kit displays RGB.
Instructions to Add Led Driver3 Functionality to the Application
The user could use this demonstration as an example to add led driver3 functionality to the MPLAB Harmony v3 based application. Follow the below steps.
- If the user has not downloaded the led driver3 demo yet Click Here to download, otherwise go to next step.
- Unzip the downloaded .zip file.
- From the unzipped folder leddriver3/firmware/src, copy the folder click_routines to the folder firmware/src under the MPLAB Harmony v3 application project.
- Open MPLAB X IDE.
- Open the application project.
- In the project explorer, Right click on
folder Header Files and add a sub folder click_routines by selecting
Add Existing Items from Folders...

- Click on Add Folder... button.

- Select the click_routines folder and select Files of Types as Header
Files.

- Click on Add button to add the selected folder.

- The led driver3 click example header files gets added to the project.

- In the project explorer, Right click on folder Source Files and add a sub
folder click_routines by selecting Add Existing Items from Folders...

- Click on Add Folder... button.

- Select the click_routines folder and select Files of Types as Source
Files.

- Click on Add button to add the selected folder.

- The led driver3 click example source files gets added to the project.

- The led driver3 click example uses the
I2C and Timer peripherals. The configuration of these
peripherals for the application depends on the 32-bit MCU and development board the user
is using.
- Configure I2C:
- Add the I2C peripheral block to the MCC project graph.
- Configure I2C Pins
using MCC Pin configuration Window.The I2C configuration depends on:
- 32-bit MCU
- 32-bit MCU development board
- The socket on which the
user has mounted the led driver3 click board
Example: The led driver3 click example on SAM E51 Curiosity Nano Evaluation Kit uses mikroBUS socket #1 on the Curiosity Nano Base for Click boards to mount the led driver3 click board. The I2C lines from MCU coming to this socket are from the SERCOM2 peripheral on the MCU.
Figure 3-14. MCC Project Graph - I2C Configuration 
Figure 3-15. MCC Pin Configurator - I2C Pin Configuration
- Configure Timer:
- Configure Timer peripheral
block in the MCC project graph.The Timer configuration depends on:
-
32-bit MCU
Example: The led driver3 click example on SAM E51 Curiosity Nano Evaluation Kit uses SysTick timer module on the MCU to implement the time requirement of led driver3 click routines.
Figure 3-16. MCC Project Graph - SysTick Configuration 
-
- Configure Timer peripheral
block in the MCC project graph.
- Map Generic Macros:
- After generating the project, following the above configuration, map the generic macros used in the click routines to the Harmony PLIB APIs of the 32-bit MCU the project is running on.
- The generic macros should be
mapped in the header file click_interface.h.

Example: The led driver3 click routines for the example on SAM E51 Curiosity Nano Evaluation Kit uses the following Harmony PLIB APIs.
The click_routines folder contain an example C source file leddriver3_example.c. The user could use leddriver3_example.c as a reference to add led driver3 functionality to the application.
- Configure I2C:
Comments
- Reference Training Module:
- This application demo builds and
works out of box by following the instructions above in Running the Demo
section. If the user needs to enhance/customize this application demo, should use the
MPLAB Harmony v3 Software framework. Refer links below to setup and build the
applications using MPLAB Harmony.
- How to Setup MPLAB Harmony v3 Software Development Framework (DS90003232).
- How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project (DS90003253).
- MPLAB Harmony v3 is configurable through MPLAB Code Configurator (MCC). Refer to the below links for specific instructions to use MPLAB Harmony v3 with MCC.