3.6.4.22 13DOF Click Example on SAM E51 Curiosity Nano Evaluation Kit
Description
This example demonstrates the reading of weather parameters (Temperature, Pressure , Humidity and Gas Resistance) from BME680 sensor, Motion parameters (Gyroscope, Accelerometer) in X , Y and Z axes from BMI088 sensor,Geomagnetic data in X , Y and Z axes from BMM150 sensor. These three sensors are integrated sensors on 13DOF Click board, these parameters are displayed on a serial terminal when the switch on SAM E51 Curiosity Nano Evaluation Kit is pressed.
Modules/Technology Used
- Peripheral Modules:
- EIC
- SYSTICK
- GPIO
- SERCOM (I2C)
- SERCOM (USART)
Hardware Used
Software/Tools Used
This project has been verified to work with the following versions of software tools:
Refer Project Manifest present in harmony-manifest-success.yml under the project folder firmware/src/config/sam_e51_cnano.
- Refer the Release Notes to know the MPLAB X IDE and MCC Plugin version.
- Any Serial Terminal application, such as Tera Term terminal application.
Because Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected. It is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).
Setup
- Mount SAM E51 Curiosity Nano Evaluation Kit on "CNANO56_HOST_CONN"(U3) connector of Curiosity Nano Base board.
- Mount 13DOF Click board on mikroBUS click 1 connector of Curiosity Nano Base board.
- Connect the SAM E51
Curiosity Nano Evaluation Kit to the Host PC as a USB Device through a
Type-A male to micro-B USB cable connected to Micro-B USB (Debug USB)
port.
Programming Hex File
The pre-built hex file can be programmed by following the below steps.
- Open MPLAB X IDE
- Close all existing projects in IDE, if any project is opened.
- Go to File -> Import -> Hex/ELF File.
- In the Import Image
File window,
- Create Prebuilt
Project,
- Click the Browse button to select the prebuilt hex file.
- Select Device as ATSAME51J20A.
- Ensure the proper tool is selected under Hardware Tool and click on Next button.
- Select Project
Name and Folder,
- Select appropriate project name and folder and click on Finish button
- Create Prebuilt
Project,
- In MPLAB X IDE, click on Make and Program Device button to program the device.
- Follow the steps in Running the Demo section below.
Programming/Debugging Application Project
- Open the project (13dof/firmware/sam_e51_cnano.X) in MPLAB X IDE
- Ensure SAM E51 Curiosity Nano is selected as hardware tool to program/debug the application
- Build the code and program the device by clicking on the Make and Program button in MPLAB X IDE tool bar
- Follow the steps in Running the Demo section below
Running the Demo
- Open the Tera Term terminal application on the PC (from the Windows Start menu by pressing the Start button).
- Set the baud rate to 115200.
- Press the switch SW0 on
the SAM E51 Curiosity Nano Evaluation Kit to print the weather
(Temperature, Pressure, Gas Resistance and Humidity), motion parameters
(Gyroscope, Accelerometer) and geomagnetic data.

- For every switch press, the SAM E51 Curiosity Nano Evaluation Kit prints the latest weather, motion and geomagnetic data parameters.
Instructions to Add 13dof Functionality to the Application
The user could use this demonstration as an example to add 13dof functionality to the MPLAB Harmony v3 based application. Follow the below steps.
- If the user has not downloaded the 13dof demo yet Click Here to download, otherwise go to next step.
- Unzip the downloaded .zip file.
- From the unzipped folder 13dof/firmware/src, copy the folder click_routines to the folder firmware/src under the MPLAB Harmony v3 application project.
- Open MPLAB X IDE.
- Open the application project.
- In the project explorer,
right click on folder Header Files and add a sub folder
click_routines by selecting Add Existing Items from
Folders...

- Click on Add Folder... button.

- Select the click_routines folder and select Files of Types as
Header Files.

- Click on Add button to add the selected folder.

- The 13dof click example header files gets added to the project.

- In the project explorer, Right click on folder Source Files and add a
sub folder click_routines by selecting Add Existing Items from
Folders...

- Click on Add Folder... button.

- Select the click_routines folder and select Files of Types as
Source Files.

- Click on Add button to add the selected folder.

- The 13dof click example source files gets added to the project.

- The 13dof click example uses
the I2C and Timer peripherals. The configuration of
these peripherals for the application depends on the 32-bit MCU and
development board the user is using.
- Configure
I2C:
- Add the I2C peripheral block to the MCC project graph.
- Configure
I2C Pins using MCC Pin configuration
Window.The I2C configuration depends on:
- 32-bit MCU
- 32-bit MCU development board
- The socket on which the user has mounted the
13dof click board
Example: The 13dof click example on SAM E51 Curiosity Nano Evaluation Kit uses mikroBUS socket #1 on the Curiosity Nano Base for Click boards to mount the 13dof click board. The I2C lines from MCU coming to this socket are from the SERCOM2 peripheral on the MCU.
Figure 3-74. MCC Project Graph - I2C Configuration 
Figure 3-75. MCC Pin Configurator - I2C Pin Configuration 
- Configure
Timer:
- Configure
Timer peripheral block in the MCC project graph.The Timer configuration depends on:
- 32-bit MCU
Example: The 13dof click example on SAM E51 Curiosity Nano Evaluation Kit uses SysTick timer module on the MCU to implement the time requirement of 13dof click routines.
Figure 3-76. MCC Project Graph - SysTick Configuration 
- 32-bit MCU
- Configure
Timer peripheral block in the MCC project graph.
- Map Generic
Macros:
- After generating the project, following the above configuration, map the generic macros used in the click routines to the Harmony PLIB APIs of the 32-bit MCU the project is running on.
- The generic
macros should be mapped in the header file
click_interface.h.

Example: The 13dof click routines for the example on SAM E51 Curiosity Nano Evaluation Kit uses the following Harmony PLIB APIs.
The click_routines folder contain an example C source file 13dof_example.c. The user could use 13dof_example.c as a reference to add 13dof functionality to the application.
- Configure
I2C:
Comments
- Reference Training Module:
- This application demo
builds and works out of box by following the instructions above in
Running the Demo section. If the user needs to
enhance/customize this application demo, should use the MPLAB Harmony v3
Software framework. Refer links below to setup and build the
applications using MPLAB Harmony.
- How to Setup MPLAB Harmony v3 Software Development Framework (DS90003232).
- How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project (DS90003253).
- Video - How to Set up the Tools Required to Get Started with MPLAB® Harmony v3 and MCC
- Create a new MPLAB Harmony v3 project using MCC
- Update and Configure an Existing MHC-based MPLAB Harmony v3 Project to MCC-based Project