3.4.3.5 Non-Cached Events
Certain fetches from the NVM are not cached. These include:
- Interrupt Vector fetches
- Fetches of debug executive code
- Fetches of invalid program memory data
All these types of fetches are not cached to avoid cache thrashing. Thrashing occurs when other useful data are evicted from the cache and replaced with less useful or invalid data. Inhibiting caching during the above fetches is expected to improve the overall efficacy of the cache, resulting in more cache hits at run time.
Interrupt Vector fetches are a special type of non-cached event. Specifically, only one program word is fetched from the NVM when the CPU indicates a vector fetch and the ISB is bypassed. When an interrupt occurs, the interrupt vector address is fetched from the vector table, then the instruction at the interrupt vector address is fetched. There is no need for an ISB to perform a prefetch and fetch the program word after the one that contains the interrupt vector address. This would be wasteful and produce extra latency in the servicing of the interrupt event.
The PBU monitors whether the CPU is executing user code or debug executive code. Instructions fetched from the debug executive code are not cached. This avoids additional indeterministic behavior when code execution transitions from the debug executive code back to user mission-mode code.
In addition, the CPU supports execution from RAM and a RAM-based Interrupt Vector Table (IVT). Program or vector fetches from RAM are also non-cached events. However, this capability introduces the possibility of both a vector and its associated handler routine being in either NVM or RAM. Whenever the IVT and/or an exception handler (interrupt or trap) are located within RAM, this is treated as a special case by the PBU to maintain efficient operation.