16.3.7 Error Reporting
LPM/LD/ST/STM). ECC
errors occurring in NVM memories are reported as follows:| Memory | Which Information? | How to know? |
|---|---|---|
| Flash Fetch or NVM Data | Single- or double-bit | INTFLAGSB |
| Word address | ADDR | |
| ECC Parity bits read from NVM | PARITY | |
| Failing bit in ECC word | SYNDROME |
The NVM controller has several parallel logical interfaces: Flash write, Flash fetch, Flash data, EEPROM write and EEPROM read. A single ECC check circuit performs all ECC checking. Therefore, these checks will be serialized, and only one of the logical interfaces can generate an ECC error at any time. Whenever an ECC error is detected, the ADDR, PARITY and SYNDROME registers are frozen, and the appropriate flags in the INTFLAGSB register are set. The ADDR, PARITY and SYNDROME registers remain frozen as long as any ECC flags in the INTFLAGSB register is set.
An LD or LPM instruction in the address in ADDR is
required to retrieve the failing word. Note that this word will already be ECC-corrected,
at least in the case of a 1-bit error, so it may appear correct even though the flags
indicate otherwise.