4.2.17 CPU STATUS Register(1)

Note:
  1. The CPU STATUS register is not memory mapped. The IPL3 bit is concatenated with the IPL[2:0] bits (SR[7:5]) to form the CPU Interrupt Priority Level.
Name: SR

Bit 3130292827262524 
          
Access  
Reset  
Bit 2322212019181716 
 VF    CTX[2:0] 
Access RRRR 
Reset 0000 
Bit 15141312111098 
 OAOBSASBOABSAB IPL3 
Access R/WR/WR/WR/WRR/CR/C 
Reset 0000000 
Bit 76543210 
 IPL[2:0]RANOVZC 
Access R/WR/WR/WRR/WR/WR/WR/W 
Reset 00000000 

Bit 23 – VF Vector (Fetch) Fail Status bit

ValueDescription
1

Indicates to the Bus Error handler that the source of the bus error is a vector fetch. The vector data read will be substituted with the contents of the Vector Fail Address (VFA) SFR.

0 Indicates to the Bus Error handler that the source of the bus error is not a vector fetch.

Bits 18:16 – CTX[2:0] Current (W register) Context Identifier bits

ValueDescription
111 Context 7 is currently in use.
110 Context 6 is currently in use.
101 Context 5 is currently in use.
100 Context 4 is currently in use.
011 Context 3 is currently in use.
010 Context 2 is currently in use.
001 Context 1 is currently in use.
000 Context 0 is currently in use.

Bit 15 – OA Accumulator A Fractional Overflow Status bit

ValueDescription
1 Accumulator A fractional overflow has occurred (its contents can no longer be represented as a 1.63 fractional value).
0 Accumulator A has not overflowed.

Bit 14 – OB Accumulator B Fractional Overflow Status bit

ValueDescription
1 Accumulator B fractional overflow has occurred (its contents can no longer be represented as a 1.63 fractional value).
0 Accumulator B has not overflowed.

Bit 13 – SA Accumulator A Saturation/Sign Overflow ‘Sticky’ Status bit

ValueDescription
1 Accumulator A is saturated, or has been saturated at some time or has overflowed into bit 71 (if saturation is disabled).
0 Accumulator A is not saturated or has not overflowed into bit 71 (if saturation is disabled).

Bit 12 – SB Accumulator B Saturation/Sign Overflow ‘Sticky’ Status bit

ValueDescription
1 Accumulator B is saturated or has been saturated at some time or has overflowed into bit 71 (if saturation is disabled).
0 Accumulator B is not saturated or has not overflowed into bit 71 (if saturation is disabled).

Bit 11 – OAB Combined Accumulator A or Accumulator B Fractional Overflow Status bit

ValueDescription
1 Accumulators A or B fractional overflow has occurred (one or both of their contents can no longer be represented as a 1.63 fractional value).
0 Neither Accumulators A nor B have overflowed.

Bit 10 – SAB Combined Accumulator A or Accumulator B "Sticky" Status bit

ValueDescription
1 Accumulators A or B are saturated, or have been saturated at some time or have overflowed into bit 71 (if saturation is disabled).
0 Neither Accumulator A nor B are saturated or have overflowed into bit 71 (if saturation is disabled).

Bit 8 – IPL3 MS-bit of CPU Priority Level Nibble bit

User mode: This bit is R/C-0 (read-only if Supervisor mode supported) and will reset to 0b0.

Supervisor mode: This bit is R/C-0 (CPU will reset into Supervisor mode).

ValueDescription
1 CPU Priority ≥ 8 (trap exception underway).
0 CPU Priority < 8 (no trap exception underway).

Bits 7:5 – IPL[2:0] CPU Interrupt Priority Level status bits

User mode: This bit is R/C-0 (read-only if Supervisor mode supported) and will reset to 0b0.

Supervisor mode: This bit is R/C-0 (CPU will reset into Supervisor mode).

ValueDescription
111 All interrupts disabled.
110 Level 7 interrupts enabled.
101 Level 6 and 7 interrupts enabled.
100 Level 5 through 7 interrupts enabled.
011 Level 4 through 7 interrupts enabled.
010 Level 3 through 7 interrupts enabled.
001 Level 2 through 7 interrupts enabled.
000 Level 1 through 7 interrupts enabled.

Bit 4 – RA REPEAT Loop Active bit

ValueDescription
1 REPEAT loop is in progress.
0 REPEAT loop is not in progress.

Bit 3 – N MCU ALU Negative bit

ValueDescription
1 Result was negative.
0 Result was not negative (zero or positive).

Bit 2 – OV MCU ALU Overflow bit

This bit is used for signed arithmetic (two’s complement). It indicates an overflow of the magnitude that causes the sign bit to change state.
ValueDescription
1 Overflow occurred for signed arithmetic (in this arithmetic operation).
0 No overflow occurred.

Bit 1 – Z ALU ‘Sticky’ Zero bit

ValueDescription
1 An operation which affects the Z bit has set it at some time in the past.
0 The most recent operation which affects the Z bit has cleared it (i.e., a non-zero result).

Bit 0 – C  ALU Carry/Borrow bit

SR[31:0] is stacked during exception processing, preserving context.