16.6.1.3 Six-Step Commutation – PWM Scheme 3
In this PWM scheme, four switches are driven in a given sector. Two pairs of complementary PWM outputs are applied to the two active phases. The inactive phase is overridden low as needed, as shown in Figure 16-44.
In this scheme, Center-Aligned PWM mode is used with dead time to prevent high current during switching transitions. The two active phases are driven 180 degrees out of phase to one another using the SWAP feature.
Configuration Summary:
- Center-Aligned PWM mode
- Complementary Output mode
- Master period and duty cycle used
- Override and SWAP state are dependent on Sector state.
- Dead time is applied to the Complementary PWM Signal.
Six-Step PWM Scheme 3 Code
//For delay function
#define FCY 8000000 //CPU frequency in Hz
#include "libpic30.h"
#include <xc.h>
#include <stdint.h>
uint32_t state = 0;
uint32_t PWMState1[6] = {0x0000000C,0x0000000C,0x0000000C,0x0000080C,0x0000080C,0x0000080C};
uint32_t PWMState2[6] = {0x00000000,0x00000000,0x00300000,0x00000000,0x00000000,0x00300000};
uint32_t PWMState3[6] = {0x0000080C,0x0000080C,0x0000000C,0x0000000C,0x0000000C,0x0000080C};
uint32_t PWMState4[6] = {0x00000000,0x00300000,0x00000000,0x00000000,0x00300000,0x00000000};
uint32_t PWMState5[6] = {0x0000000C,0x0000080C,0x0000080C,0x0000080C,0x0000000C,0x0000000C};
uint32_t PWMState6[6] = {0x00300000,0x00000000,0x00000000,0x00300000,0x00000000,0x00000000};
void PWMInitialization(void);
int main(void)
{
PWMInitialization();
/* To Update Duty cycle values to PG1-PG3, add two lines of code written
below (In this example, setting 50% Duty Cycle):
After writing the MDC register, set the Update request bit PG1STATbits.UPDREQ.
This will transfer the MDC value to all the PWM generators PG1-PG3.
Note that the Update Mode (UPDMOD) of PG2, PG3 is Client EOC and
PG1 MSTEN bits is '1' */
PG1STATbits.UPDREQ = 1;
while (1)
{
for (state=0; state<6;state++)
{
/* Delay is used to simulate BLDC commutation; In practical
application, commutation state transition will be based on feedback from Motor */
__delay_us(200);
PG1IOCON1 = PWMState1[state];
PG1IOCON2 = PWMState2[state];
PG2IOCON1 = PWMState3[state];
PG2IOCON2 = PWMState4[state];
PG3IOCON1 = PWMState5[state];
PG3IOCON2 = PWMState6[state];
}
}
}
void PWMInitialization(void)
{
PCLKCON = 0x0000;
//Set PWM master clock to 400MHz from PLL2 through CLKGEN5
configure_PLL2_Fout_400MHz();
clock_PWM_from_PLL2_Fout();
/* PWM Clock Divider Selection bits
0b11 = 1:16 ; 0b10 = 1:8 ;0b01 = 1:4 ; 0b00 = 1:2 */
PCLKCONbits.DIVSEL = 0;
/* PWM Master Clock Selection bits
0b01 = CLKGEN5 ; 0b00 = UPB clock */
PCLKCONbits.MCLKSEL = 1;
/* Lock bit: 0 = Write-protected registers and bits are unlocked */
PCLKCONbits.LOCK = 0;
/* Initialize Master Period Register */
MPER = 40000;
/* Initialize Master Duty Cycle */
MDC = 20000;
/* Initialize PG1CON Registers */
PG1CON = 0x00000000;
/*PWM Generator uses the master clock selected by the MCLKSEL[1:0]
* (PCLKCON[1:0] control bits */
PG1CONbits.CLKSEL = 1;
/* Select PWM Generator duty cycle register as MDC */
PG1CONbits.MDCSEL = 1;
/* Select PWM Generator period register as MPER */
PG1CONbits.MPERSEL = 1;
/* PWM Generator broadcasts software set of UPDREQ control bit and EOC signal
* to other PWM Generators. */
PG1CONbits.MSTEN = 1;
/* Start of cycle is local EOC */
PG1CONbits.SOCS = 0b0000;
/* PWM Generator operates in Center-Aligned PWM mode*/
PG1CONbits.MODSEL = 4;
/* Initialize PG1IOCON Registers */
PG1IOCON1 = 0x00000000;
/* PWM Generator Output Mode is Complementary Mode */
PG1IOCON1bits.PMOD = 0;
/* PWM Generator controls the PWMxH output pin */
PG1IOCON1bits.PENH = 1;
/* PWM Generator controls the PWMxL output pin */
PG1IOCON1bits.PENL = 1;
PG1EVT1 = 0x00000000;
/* A write of the PGxDC register automatically sets the UPDREQ bit */
PG1EVT1bits.UPDTRG = 0;
/* PWM generator trigger output is EOC*/
PG1EVT1bits.PGTRGSEL = 0;
/* Initialize PG2CON Registers */
PG2CON = 0x00000000;
/*PWM Generator uses the master clock selected by the MCLKSEL[1:0]
* (PCLKCON[1:0] control bits */
PG2CONbits.CLKSEL = 1;
/* Select PWM Generator Duty Cycle Register as MDC */
PG2CONbits.MDCSEL = 1;
/* Select PWM Generator Period Register as MPER */
PG2CONbits.MPERSEL = 1;
/* Start of Cycle is PG1 trigger output selected by
* PG1EVTbits.PGTRGSEL<2:0> bits */
PG2CONbits.SOCS = 0b0001;
/* PWM Generator operates in Center-Aligned PWM mode*/
PG2CONbits.MODSEL = 4;
/* Initialize PG2IOCON Registers */
PG2IOCON1 = 0x00000000;
/* PWM Generator Output Mode is Complementary Mode */
PG2IOCON1bits.PMOD = 0;
/* PWM Generator controls the PWMxH output pin */
PG2IOCON1bits.PENH = 1;
/* PWM Generator controls the PWMxL output pin */
PG2IOCON1bits.PENL = 1;
/* Initialize PG3CON Registers */
PG3CON = 0x00000000;
/*PWM Generator uses the master clock selected by the MCLKSEL[1:0]
* (PCLKCON[1:0] control bits */
PG3CONbits.CLKSEL = 1;
/* Select PWM Generator Duty Cycle Register as MDC */
PG3CONbits.MDCSEL = 1;
/* Select PWM Generator Period Register as MPER */
PG3CONbits.MPERSEL = 1;
/* Start of Cycle is PG1 trigger output selected by
* PG1EVTbits.PGTRGSEL<2:0> bits */
PG3CONbits.SOCS = 0b0001;
/* PWM Generator operates in Center-Aligned PWM mode*/
PG3CONbits.MODSEL = 4;
/* Initialize PG3IOCON Registers */
PG3IOCON1 = 0x00000000;
/* PWM Generator Output Mode is Complementary Mode */
PG3IOCON1bits.PMOD = 0;
/* PWM Generator controls the PWMxH output pin */
PG3IOCON1bits.PENH = 1;
/* PWM Generator controls the PWMxL output pin */
PG3IOCON1bits.PENL = 1;
/* Initialize PWM GENERATOR 3 DEAD-TIME REGISTER */
PG3DT = 0x06400640;
/* Initialize PWM GENERATOR 2 DEAD-TIME REGISTER */
PG2DT = 0x06400640;
/* Initialize PWM GENERATOR 1 DEAD-TIME REGISTER */
PG1DT = 0x06400640;
/* Enable PWM generator 3 */
PG3CONbits.ON =1;
/* Enable PWM generator 2 */
PG2CONbits.ON =1;
/* Enable PWM generator 1, starting all PWM generators together */
PG1CONbits.ON =1;
}