16.5.2.3.3 Push-Pull Output Mode
The Push-Pull Output mode is similar to Independent Edge mode, however, the PWM cycle, as defined by the MODSEL[2:0] bits, is repeated twice each time a SOC trigger is received. The EOC trigger event and updates from Data registers are held off until the end of the second PWM cycle. Figure 16-17 shows the 2nd cycle that is invoked when using Push-Pull Output mode.
Operating the PWM in Push-Pull mode will double the period for a complete cycle, as there are two timer matches per cycle. If PGxTRIGy timers are used for event timing, the STEER signal can be used to gate application timing.
Push-Pull PWM mode is typically used in transformer coupled circuits
to ensure that no net DC currents flow through the transformer. Push-Pull mode ensures that
the same duty cycle PWM pulse is applied to the transformer windings in alternate
directions. The phase of the push-pull count period can be determined by reading the STEER
status bit (PGxSTAT[2]). If STEER = 0, the PWM
Generator is generating the first PWM pulse. If STEER = 1, the PWM Generator is generating the second PWM pulse.
Since dead time is not available in Push-Pull mode, delays can be emulated in the Push-Pull Output mode by introducing a small phase offset with the PGxPHASE register. Similarly, the maximum duty cycle may be limited in software to avoid a pulse that ends too close to the start of the next PWM cycle.
Push-Pull Operation with Center-Aligned Modes
When the PWM Generator is operated in one of the two Center-Aligned modes, and the Push-Pull mode is selected, a complete PWM cycle will comprise four time base cycles.
Figure 16-18 shows the operation
of the module with Push-Pull Output mode and Center-Aligned PWM mode. This combination of
modes limits PWM buffer updates and interrupt events to every fourth time base cycle.
Therefore, the same pulse is produced on the PWMxH and PWMxL pins before any changes to the
duty cycle are allowed. Similar interrupt behavior also occurs when Dual Edge
Center-Aligned mode (one update per cycle) is selected (MODSEL[2:0] = 110).
110)Figure 16-19 shows the operation
of the module with Push-Pull Output mode and Dual Edge Center-Aligned PWM mode (two updates
per cycle, MODSEL[2:0] = 111) or Double Update
Center-Aligned mode. This combination of modes allows a buffer update and interrupt event
on every time base cycle. This operating configuration does not attempt to maintain
symmetrical pulses on the PWMxH and PWMxL outputs, which is a requirement for many
push-pull applications. User software can change the edge times of the center-aligned
pulses after every edge event, which minimizes control loop latency.
111)