44.4 OPA Operation with ADC
When INTOE
                                    = 1, the OPA module provides internal
                                    connections directly to the ADC, allowing it to be used for
                                    analog signal conditioning before a signal is converted by the
                                    ADC. In this mode of operation, the external output of the OPA
                                    connected to the OPAxOUT pin is disabled, and the internal
                                    output of the OPA module is available to be selected as an ADC
                                    input through the ADC channel selection register. When using
                                    this mode of operation, the ADPCH register of the ADC module
                                    must be used to select one of the available OPA input pins. The
                                    OPA input pin selection determined using the ADC input channel
                                    selection register will take precedence over the input pin
                                    selection using the PSS bits. The noninverting OPA input
                                    will switch to the pin selected by the ADPCH, and the OPA output
                                    will be connected to the ADC input.
1, the external output of the OPA
                                                module is disabled and the OPAxOUT pin can be used
                                                as a GPIO.