1.3.2.3.22 MAC_WRP_StartRequest Function
C
void MAC_WRP_StartRequest
(
MAC_WRP_HANDLE handle,
MAC_WRP_START_REQUEST_PARAMS *startParams
);
Summary
The MAC_WRP_StartRequest primitive starts a G3 Network and sets the device as the PAN Coordinator.
Description
Start operation asks MAC layer(s) to start a G3 Network, turning the device into the PAN Coordinator of such Network, and setting the PAN Identifier. Result is provided in the corresponding Confirm callback.
Precondition
A valid handle has to be obtained before calling this function, by means of MAC_WRP_Open function.
Parameters
| Param | Description |
|---|---|
| handle | A valid handle which identifies the Mac Wrapper instance |
| startParams | Pointer to structure containing required parameters for request. See MAC_WRP_START_REQUEST_PARAMS. |
Returns
None.
Example
// ... MAC_WRP_HANDLE handle; handle = MAC_WRP_Open(G3_MAC_WRP_INDEX_0, MAC_WRP_BAND_CENELEC_A); // ... MAC_WRP_START_REQUEST_PARAMS params = { .panId = 0x1234 }; MAC_WRP_StartRequest(handle, ¶ms); // Wait for Start Confirm
Remarks
This primitive is only used by the PAN Coordinator node, which is the one in charge of Starting the PAN.