1.3.2.3.38 MAC_WRP_HANDLERS Struct

C

typedef struct
{
    /* Callbacks */
    MAC_WRP_DataConfirm dataConfirmCallback;
    MAC_WRP_DataIndication dataIndicationCallback;
    MAC_WRP_ResetConfirm resetConfirmCallback;
    MAC_WRP_BeaconNotifyIndication beaconNotifyIndicationCallback;
    MAC_WRP_ScanConfirm scanConfirmCallback;
    MAC_WRP_StartConfirm startConfirmCallback;
    MAC_WRP_CommStatusIndication commStatusIndicationCallback;
    MAC_WRP_SnifferIndication snifferIndicationCallback;
} MAC_WRP_HANDLERS;

Summary

Set of Event Handler function pointers to receive events from MAC Wrapper.

Description

Defines the set of callback functions that MAC Wrapper uses to generate events to upper layer.

Field description:

  • dataConfirmCallback: Pointer to function to be called when a Data Transmission is finished on MAC Wrapper. See MAC_WRP_DataConfirm.
  • dataIndicationCallback: Pointer to function to be called when a Data frame is received by MAC Wrapper. See MAC_WRP_DataIndication.
  • resetConfirmCallback: Pointer to function to be called when a Reset is finished on MAC Wrapper. See MAC_WRP_ResetConfirm.
  • beaconNotifyIndicationCallback: Pointer to function to be called when a Beacon frame is received by MAC Wrapper. See MAC_WRP_BeaconNotifyIndication.
  • scanConfirmCallback: Pointer to function to be called when a Scan process is finished on MAC Wrapper. See MAC_WRP_ScanConfirm.
  • startConfirmCallback: Pointer to function to be called when a Start process is finished on MAC Wrapper. See MAC_WRP_StartConfirm.
  • commStatusIndicationCallback: Pointer to function to be called when a Comm Status event occurs on MAC Wrapper. See MAC_WRP_CommStatusIndication.
  • snifferIndicationCallback: Pointer to function to be called when any frame is received MAC Wrapper. Only invoked if MAC Sniffer is enabled by corresponding PIB. See MAC_WRP_SnifferIndication.

Remarks

In case an event is to be ignored, setting its corresponding callback function to NULL will lead to the event not being generated.