1.3.2.3.16 MAC_WRP_ResetConfirm Typedef
C
typedef void (*MAC_WRP_ResetConfirm)(MAC_WRP_RESET_CONFIRM_PARAMS *rcParams);
Summary
Pointer to a Reset Confirm Event handler function.
Description
This data type defines the required function signature for the MAC Wrapper Reset Confirm event handling callback function. A client must register a pointer using the event handling function whose function signature (parameter and return value types) matches the types specified by this function pointer in order to receive Reset Confirm events back from module.
Parameters
| Param | Description |
|---|---|
| rcParams | Pointer to structure containing parameters related to Confirm. See MAC_WRP_RESET_CONFIRM_PARAMS. |
Returns
None.
Example
App_ResetConfirm(MAC_WRP_RESET_CONFIRM_PARAMS *params)
{
// Check result
if (params->status != MAC_WRP_STATUS_SUCCESS)
{
// Handle Reset error
}
else
{
// Reset performed correctly
// Reinitialize MAC Wrapper module
}
}
Remarks
None.