1.3.2.3.55 MAC_WRP_POS_ENTRY_RF Struct

C

typedef struct __attribute__((packed))
{
    MAC_WRP_SHORT_ADDRESS shortAddress;
    uint8_t forwardLqi;
    uint8_t reverseLqi;
    uint8_t dutyCycle;
    uint8_t forwardTxPowerOffset;
    uint8_t reverseTxPowerOffset;
    uint16_t posValidTime;
} MAC_WRP_POS_ENTRY_RF;

Summary

The MAC RF POS Table Entry as defined in the G3-PLC standard.

Description

This structure contains the fields that define a MAC RF POS table entry as defined in the G3-PLC standard. POS table contains an entry for every node a frame has been received, either addressed for us or not.

Field description:

  • shortAddress: Short Address of node in the hearing domain
  • forwardLqi: Link Quality reported by neighbour when receiving the frames
  • reverseLqi: Link Quality of last received frame from node
  • dutyCycle: Current Duty Cycle consumed by neighbour node
  • forwardTxPowerOffset: TxPowerOffset used to transmit to neighbour node
  • reverseTxPowerOffset: TxPowerOffset used by neighbour node when transmitting towards us
  • posValidTime: Time left, in seconds, for the entry to expire

Remarks

It is only used when RF MAC layer is present.