4.3.2 Reading Endpoint DIP SW Status

To read the DIP SW Status, click Enable DIP SW Session button, as shown in the following figure.

Figure 4-7. DIP SW Status Option

The GUI initiates the DIP switch status read request. As a result, the DIP SW status on the Endpoint board is displayed, as shown in the following figure. Change the DIP SW positions on the Endpoint board and observe the same in GUI.

Figure 4-8. Endpoint DIP SW Status